用LM358做了一个电压检测电路,发现运放正向输入和反向输入有9mV误差,减小分压电阻,压差变成1mv
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
这里应该是运放输入偏置电流在分压电阻上产生输入失调电压造成的结果,LM358输入偏置电流典型值20nA,最大值250nA,这个电流在100K电阻上产生的失调电压是20nA*100kΩ~250nA*100kΩ,即2mV~25mV;而在10K电阻上产生的失调电压是0.2mV~ 2.5mV,它们相差10倍,与您测得的9mV和1mV基本一致。
更多关于输入偏置电流和失调电压的信息,请查看帖子: