This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL071B: 使用TL071B设计电流检测电路

Part Number: TL071B

大家好,请教个问题,使用TL071B设计电流检测电路,电流0-1A,输出电压对应0-1V,直流传输特性曲线一直不符合预期,是什么原因?  未改动.TSC

  • 您好,

    这应该是输入信号范围不满足输入共模电压要求造成的,看TL071BC电气特性截图,在±15V供电时,输入共模电压范围典型值是–12 to 15V,因此是达不到负电源轨的,与负电源轨有3V的距离。因此在单电源供电时,输入共模电压至少在3V以上。

    我将上述电路改为±12V供电后,输入0~1A电流,使用50mΩ电阻,放大100倍,产生0~5V电压,如下截图所示,是线性工作的。