我通过LMV358IDR运放进行电流采样,空载时计算出来的基准电压为0.6V放大倍数为28倍,但是这批次问题是运放空载时计算出来的电压会小于0.5V或大于0.7V,误差较大
能问一下为什么么

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
明白了,在空载时,电路相当于同向比例放大电路,放大倍数28倍。
运放的输入失调电压最大值是7mV,同向端输入电压计算大概为21.2mV,加上7mV的输入失调电压,放大28倍,输出可以到784mV。因此有的运放输出到达0.7V是正常的范围。

LMV358输入失调电压只有正的,输出电压到达0.5V的可能性是3.3V电压的稳定性,如果3.3V电压偏低,那么同向输入端的分压就会偏低进而导致输出偏低,因此这里建议您用示波器同时测量同向端输入信号和输出信号的变化,以确认是否同上输入端电压偏低造成的?
另外,分压电阻和运放比例电阻的精度也有影响。