This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THS3491: THS3491额定增益是5V/V, 能否提高增益。 最大增益可以到多少

Part Number: THS3491


我现在需要做一个430mA, 100Mhz输出。 5V/V的增益是否是5倍的放大。能否把这个增益提高。最大增益可以到多少

谢谢

  • 您好,

    是的, 5V/V的增益是5倍的放大。

    您输入信号的电压幅值是多少?您期望的输出电压幅值是多少?

    THS3491是电流型反馈放大器,其带宽仅与反馈电阻RF有关。因此其工作带宽与RF/RG的比值没有关系,但是其输出幅值要满足其压摆率SR的限制。

  • 我输入的电压是200毫伏。负载阻抗是50OHM。 电流需要430毫安输出。输出频率是100Mhz。 是否意味着输出电压要到20V。如果是20V的话,我的放大倍数需要100倍?

    谢谢

  • 输出电流越大,输出电压降越大,下面分别是±15V(图31)和±7V(图59)不同输出电流下的电压降:

    如果您要输出20V的话,THS3491压摆率是8000V/µs (VO = 20VPP),而需求的SR=2π*f*Vpp=12560V/us,THS3491的压摆率SR是不满足要求。