Other Parts Discussed in Thread: OPA2690, OPA690
尊敬的专家您好:
我是一个初学者,首先问一个基础问题:OPA2690是否可以等效的看过2片OPA690(不考虑disable端口)?
其次, 我尝试使用针对OPA690的一个放大2倍的反相比例放大电路进行测试:
正相输入端通过一个146欧姆的电阻接地,Rf=400欧姆,输入电阻RG=200欧姆,输入信号通过67欧姆电阻接地,输出电阻为50欧姆。供电为正负5V,正负电源之间接0.1uf电容滤波,并且分别接了0.1uf和10uf电容接地滤波。
在实际使用中,信号似乎只通过输入电阻,反馈电阻,输出电阻形成一个衰减过程,并没有通过OPA2690芯片。输入信号不变,芯片供电与否对输出信号并无影响。请问各位专家为什么会这样?如果要用2690实现2倍放大的话应该如何接电路?