请问一下VCA810和其他运放级联的时候有什么参数要求啊?我将OPA228接反比例放大电路(放大10倍)和VCA810都单独调试好之后(可实现-30db到+30db),级联起来进行仿真是正常的,但制作实际电路时,VCA810就只能放大一点几倍了。各位老师,请指点一下,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,
1.两级级联后要求运放能将测试输入的20mVpp正弦波放大-20到+40db可调;
2.两级级联后,输入20mVpp正弦波,调节VCA810的控制端电压在0到—1.2V之间,最终可输出放大或缩小的正弦波。超过—1.2V,如1.3V,则波谷开始失真(单独测试VCA810控制电压可达到-1.8V才开始出现这种失真);
3.至于R1至今用途不明确,但曾尝试撤去或替换R1。撤去R1时,增益控制极限降低为—1V,超过此值则出现失真(同上);改R1为50欧,则单独测试VCA810时,增益极限不到—1.6波峰开始失真;改R1为10欧时,输入信号基本衰减,不能得到输出(10欧和25欧阻值很小,用万用表测试相当于导线)。
对于,这个电路的确是TI给的典型应用,但效果更差,更供正5v电压后,还不如不供,虽然我用的是面包板,但我只测几k的都不行