Other Parts Discussed in Thread: OPA132, OPA656
做了一个信号放大器,就是模电书上最简单的那种—同相比例放大,芯片是OPA132,放大1000Hz信号,输出的放大信号很漂亮。我想放大10MHz的信号,就换了个增益带宽积大的芯片OPA656,结果输出什么都不是,把输入信号改成1000Hz,输出也不对,是不是OPA656有特殊的要求,求大神指点
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请注意:在相同电源供电条件下,OPA656的输入输出信号范围要小于OPA132。
所以从你的描述来看,最可能的就是输入输出信号范围的问题。
最好能把电路贴上来,要么请提供:
1.运放供电电压;
2. 输入信号电压范围
3. 电路的gain多大
假如需要放大10MHz的信号频率,放大10dB,OPA132能做到吗?