在这个条件小,如果输入》11vpp,衰减10倍,电路能不能工作?输出信号会不会失真?
如果输入9Vpp呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
THS7001没有特殊声明
absolute maximum ratings over operating free-air temperature (see Notes 1 and 2)†
Supply voltage, VCC . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . ±16.5 V
Input voltage, VI . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . ±VCC
Output current, IO (preamp) (see Note 1) 150 mA . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . IO (PGA) (see Note 1) 85 mA