Other Parts Discussed in Thread: INA128
我遇到一个这样问题,就是刚上电时运放输出的信号时正常的,不过信号的峰值会慢慢衰减到没有,然后就一直没有波形了.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
It operates with power
supplies as low as ±2.25V, allowing use in battery
operated and single 5V supply systems。这是在IN114数据手册上找到的,看IN128和IN114内部结构基本相同,应该也能够单电源供电吧,如果交流放大时,建议在ref端加VCC/2的偏置
你好,
1、一般在手册中说明要单电源供电的芯片,双电源供电是没问题的;不过双电源供电的芯片在单电源下工作这就不一定能行,得你自己去试验。
2、在放大电路中,GND相当于是一个参考点,例如正负2.5V供电时候,交流放大输出的电压信号摆幅就是以GND为中心对称,摆幅小于等于正负2.5V。
如果改为单电源5V供电,那么你的输出电压摆幅范围是0-5V,输出信号会以2.5V为对称中心摆动,所以输出就会有2.5V的直流偏置。如果不希望得到这样的结果,
在输入端加上VCC/2的直流偏置,就会将摆动中心重新搬回到GND.
希望可以帮到你。