Other Parts Discussed in Thread: OP07, INA128
我采用8颗OP07做差分放大(前级都有一级跟随),工作电源为+-15V,现在发现工作起来芯片的温度应该有40多度,这是否正常?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
10几度的温升不算高。
你算下芯片的总功耗,对应到你用的封装散热能力上,就可以大概计算出温升。
其数据手册中有“These devices are characterized for operation from 0°C to 70°C.” 因此芯片在此情况下工作并没有问题。
您好,关于您的这个问题跟您的负载和电路结构有关系的,如果您的负载较大,加上OP07的本身静态功耗,芯片温度较环境温度上升十几度都是很正常的。但是使用这种方式设计差分放大器在大多数场合下不是很科学的,首先差分放大器最重要的参数是共模抑制比,这个参数跟差分放大器的电阻精度有很大关系,例如如果您使用0.1%的电阻,共模抑制比只能达到60dB,即使使用0.01%的电阻也只能达到80dB左右,但是0.01%的电阻价格极高。所以这种情况下建议你使用仪表放大器,例如INA128等,这种仪表放大器不仅拥有高达120dB的共模抑制比(放大倍数为100时),而且拥有良好的直流精度和噪声特性,并且功耗很低,价格也很低(相对您的电路成本),所以建议您看一看相关的资料和芯片手册。
所以像你电路的这种情况,建议使用一路仪表放大器完成差分放大,一路普通精密运放完成电压跟随和放大,这样不仅提高了性能,也降低了成本和PCB的尺寸。
您好,关于您的问题我想再补充一些,你使用的OP07在正负15V供电没有负载的情况下功耗大约为0.1W左右,您电路中所带的负载很轻,几乎可以忽略,如果您用的是DIP8的封装话,其热阻为100℃/W,那么静态功耗所造成的温升约为10℃;如果您用的是SO8的封装的话,其热阻为160℃/W,那么静态功耗所造成的温升约为16℃;如果您的IC所处的环境为25℃,然后加之周围环境散热不太好的话,OP07的温度达到40℃是很正常的。我这里只是给出简单的热阻分析,实际情况您需根据你的环境及散热情况仔细分析。总之大体上,应该是正常的。