This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在用作末级电流扩流时,由于手上没有ths3120,,可否用ths3001代替?
楼主你好。
1、这个要看你自己的需要了,THS3001最大输出电流时100mA,而THS3120的最大输出电流时475mA
2、输出端扩流的话,建议你用晶体管扩流
作末级末级扩流的话,不建议直接替换。如果输出电流过高。频率幅值又高的话,可能会引起THS3001发热严重。
是否能替代,一定要根据你的具体应用来看。
两者在带宽和输出电流上的区别还是很大的。
楼主你好!
1、请问输入信号和输出信号幅值是多少?
2、信号带宽是多少?
3、典型案例是,THS3001在安X伦、普X公司的信号源上有实用。实用多颗并联均流输出。
谢谢你的提醒