This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

比较器范围

请教一下各位专家:

         我制作了一个比较器,正端输入信号,负端输入直流参考电位。正端与输出端连接了一个8.2M欧电阻和一个50p电容的并联,输出的类方波信号在200KHz~6MHz时,示波器可以获得准确的信号频率,超过了这个范围示波器不能采得准确信号。

增大并联电容的容值上限频率减小,下限频率也减小;减小并联电容容值上限频率增大,下限频率也增大。

我不清楚RC并联在反馈回路为什么会造成这样的影响,所以想请教专家其中的原理。

还想再问一下如果我想获得10Hz~10MHz的比较范围,应该怎么处理?  

PS:当反馈回路只有电阻时,示波器测量稳定的频率范围是DC~200KHz