This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好!
我这边使用THS7530做VGA,再加一级THS4541做BUFF差分输出,就是这样的一个DEMO板进行底噪测试。
测试工具为示波器:1G采样率,带宽200M,本身100+uV.
测试方案:
1、输入VGA信号对地。测量BUFF差分输出噪声。
2、断开二级BUFF,测量一级VGA输出噪声。
3、断开一级VGA,将二级BUFF输入对地,测量二级BUFF输出噪声。
测试结果:
1、差分输出噪声1.2mV(匹配电阻分压的问题,真正输出噪声为2.4mV)。
2、VGA输出噪声2.1mV。
3、BUFF输出噪声0.13mV(匹配电阻分压的问题,真正输出噪声为0.26mV)。
跟芯片的数据手册上的输入噪声对比:
THS7530理论值:200MHz^0.5 * 1.1nV/Hz^0.5 = 0.016mV,这个值跟我实测出来的值差距较大。
THS4541理论值:200MHz^0.5 * 2.2nV/Hz^0.5 = 0.035mV,而实际值为0.26mV-0.1mV(示波器噪声)=0.13mV,这个值还是比较接近理论值的。
现在我想提出的问题是:THS7530测试出来的值为什么比理论的值差距这么大?
DEMO板框图:
您好,
很抱歉回复这么晚!
电路前面您使用电阻分压的方式产生2.5V共模电压,这里的电阻也会产生噪声,因此您测量的噪声也包含了电阻的噪声。
电路增益您设置的是多少?如果增益不是1,输入噪声与输出噪声还存在增益关系;
并不是所有频带上的噪声都是1.1nV√Hz,是>100KHZ时的,同时它还有1/f噪声,下面系列视频噪声2-3-4,讲了噪声的计算方法:
https://edu.21ic.com/video/2543
下面视频讲了示波器和频谱分析仪测量噪声的方法和一些注意事项,也希望您看下哪里有操作不当的地方: