This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

这两个差分电路有什么区别?一般使用的注意事项有什么?

Other Parts Discussed in Thread: INA105, INA128

  • 您好,准确的来说,您给的两个电路中,第一个是差动放大器,第二个是仪表放大器。差动放大器有由普通运放和四颗匹配电阻组成,功能是放大两个输入端的差值,使用这个电路需要注意两个事项:1,差动放大器输入电阻很小,就是等于R1,因此差动放大器不允许信号有内阻,否则将会引起较大的误差;2,差动放大器要求电阻匹配,即R1=R3,R2=R4,以提高共模抑制比,例如如果使用0.1%的电阻,差动放大器的共模抑制比约为60dB,如果精度更差,共模抑制比就会更差。如果您要用差动放大器,推荐您使用INA105等这种集成差动放大器,其内部拥有极高精度的陪陪电阻,使其共模抑制比高达80dB以上。

    至于仪表放大器,实际上就是差动放大器加上前级放大电路组成,这样做的优点有两点:1,提高了输入阻抗,允许放大高阻信号;2,提高了放大器倍数,差动放大器放大倍数一般不大,多为几倍到十几倍,而仪表放大器可以高达10000倍。自己搭建仪表放大器电路复杂,电阻要求精度极高,成本和功耗都很高,因此建议您使用集成仪表放大器,例如INA128等,这种集成仪表放大器精度高,价格低,噪声低,功耗也低。非常适合放大各种差模小信号。