Other Parts Discussed in Thread: TL714, LMV7239
各位大神们,请问你们家TI的TL714高速比较器怎么也没有一个怎么使用的图啊?求教啊?谢谢啦!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
就一个比较啊,你要实现什么功能?
你可以参考下LMV7239的datasheet,里面有各种应用的电路图。
The TL714C is a high-speed differential comparator fabricated with bipolar Schottky process technology. The circuit has differential inputs and a TTL-compatible logic output with symmetrical switching characteristics. The device operates from a single 5-V supply and is useful as a disk-memory read-chain data comparator.
比较器没有反馈回路,所以相对运放来说比较简单,TL714这款比较器操作频率比较高,可达到50Mhz。8个引脚,一个差分输入端IN+,IN-,一个电源端VCC可接5V,GND端,输出端OUT,其他引脚可直接悬空即可。
就是一个比较器啊,NC脚悬空,接上电源,其他输入和输出就跟其他所有的比较器一样啊。如下图:
具体参数请参考:http://www.ti.com.cn/cn/lit/ds/slcs015a/slcs015a.pdf
希望对你有帮助。
负向端接要比较的参考电平,同相端输入信号注意要满足比较器的输入共模电压范围,建议您可以先做个电路,然后使用TINA进行仿真,便于你的理解。
请问 我的TL714 反向端接2.5v参考电压 同相端输入信号输出加上拉电阻在低频的时候输出波形是正常的方波但是输入一两百k的时候输出就有各种毛刺 输入给单片机,单片机也不能检测