Other Parts Discussed in Thread: LMV7239
下表红色框中,IL=-4mA,VID=-500mV和IL=-0.4mA,VID=-500mV中,这个-4mA和-0.4mA是什么电流,-500mV是什么电压,以及后面的TYP=230mV是什么意思,这些数据是怎么来的,请高手帮忙解答,谢谢。

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
IL=-4mA 和IL=-0.4mA是指的当比较器输出低电平时灌入的电流,由于LMV7235 输出是OD输出,它没有Output Swing High参数,这个参数由外部上拉电压决定,如下截图中的V2+。TYP=230mV是比较器的最低输出电压摆幅。由于输出是开关管,开关管导通时有导通电阻,因此灌入的电流越大,降在导通电阻上的电压越高,因此最低输出电压也越高。
VID是比较器的差分输入电压。

LMV7239是 push-pull输出,因此它有Output Swing High这个参数。同理,IL=4mA 和IL=0.4mA是比较器LMV7239输出高电平时的拉电流,拉电流越大,降在上管导通电阻上的电压也就越大,最大输出电压也就随之降低。