This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

opa544的做电压供应问题

Other Parts Discussed in Thread: TLV5638, OP07, OPA544, OPA277

有tlv5638  DA转换后,然后通过该电路。以实现电压可控输出。

但是,无论DA如何改变,,输出都是钳在10.12v

 

而且前面op07输出为反电压。

请大家能给出比较的好的分析,和修改意见。(Ps:opa544我是用正负12V供电的,只要求能输出0-10V就OK了。不知,直接用opa544接DA输出行不行)

  • 您好,可以直接用OPA544接DA输出的,而且建议您这样接,因为两级放大器的连接可能会引起不稳定的,因为OPA544的交直流性能都很好,所以您可以直接接DA,完全可以不需要前级的OP07.当然如果您想通过前级放大器进一步提升整体功放的性能的话,推荐您一个电路:

    图中放大器用的是OPA277和OPA512,您可以参考一下。

  • 能详细点吗,比如说:用几V供电,或者Ei  和  Eo  关系,还有电容的作用?谢谢

  • 楼主你好!

    1、OP07的作用完全是多此一举;

    2、opa544直接接DAC输出即可。