This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMC660输出震荡



     (1). Schematics: from below ,  you can see situation of application, AIB2 is input analog voltage :0-10V, VOLT_ADC is output voltage :0-1.81V.

 

 

  (2). Different batch IC

Description 2

Name

Part number

Quantity

Manufacturing date

Status

70CPE02358

NATIONAL SEMICONDUCTOR

LMC660AIMX/NOPB

2500

2013/1/4

Stock: 2384

70CPE02358

NATIONAL SEMICONDUCTOR

LMC660AIMX/NOPB

1550

2010/10/18

Used up

70CPE02358

NATIONAL SEMICONDUCTOR

LMC660AIMX/NOPB

550

2010/12/30

Used up

 

We used the batch(2010/10/18 and 2010/12/30), when input voltage(AIB2) is 4Vdc,  the voltage output(VOLT_ADC) after Amp is stable(yellow is amp output). It is good!

 

 

When supplier changed to new batch(2013/1/4) which is used for the first time, when input voltage(AIB2) is also 4Vdc, the voltage output(VOLT_ADC) after amp is not stable(yellow), output voltage occurred oscillation ! Freq=1.4MHz, AM=160mV.

 

 

            Why using the same IC which batch is only different, the output voltage  occurred oscillation? Please give us some support about this issue as soon as possible!  Thanks!