This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

运放OPA551不接负载也发热

Other Parts Discussed in Thread: OPA551

OPA551做射随用 输入10V 输出10V  供电给的是正负15V 我没接负载 输出电压正常 但是芯片上电后非常热 烫手  是怎么回事?


  • 您好,首先分析一下静态功耗,OPA551的在正负30V供电下,静态电流为7mA左右,在正负15V下只会小于等于这个值,那么静态的功耗小于等于0.2W,如果没有散热的话,DIP8封装的芯片会上升20度左右,而DDPAK封装的芯片会伤心13度左右。如果说您的芯片温升在这个范围那么就是正常的。

    另一方面,运放的输出是不能直接驱动10uF的容性负载的,否则运放电路会震荡,您可以参照附件中OPA551驱动容性负载能力,在增益为1时,其驱动1nF的负载就会出现60%的过冲,即已经不再稳定了。当运放电路震荡时也会增加功耗,所以建议您去掉输出端的电容再试试看。

     

x 出现错误。请重试或与管理员联系。