This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于由OPA735和OPA140组成的两级放大电路的问题

Other Parts Discussed in Thread: OPA140, OPA735, OPA211

      你好,我最近利用OPA735和OPA140组成的一个两级耦合放大电路,第一级放大82倍,第二放大5600倍,当没有输入时,输出在几个小时后悔自动变成高电平,这是为什么?

  • 您好,我觉得您的增益设置不是很科学,首先看一下直流特性,您的末级电路放大倍数是5600,其失调电压最大120uV,温漂最大1uV/℃,也就是说即使不考虑其他因素的影响,输出就会有672mV左右的输出,而且这个输出会伴随5.6mV/℃的温漂;其次看早上,您的总增益高达40万倍,而且没有带宽限制,这样即使以第二级电路为前置放大器计算,其输出噪声也是高得吓人,而且直接导致运放不能稳定工作的。

    不知道您为什么要放大这么大的放大倍数,这么高增益的放大器设计要非常谨慎的,首先前置放大器一定要选用极低噪声的放大器,例如OPA211;其次每一级的增益不能太大,不然失调,温漂的影响太大,而且很难稳定工作;最后想这么高增益的放大器一定要配合适当的滤波器,降低您的带宽,从而保证良好的噪声特性。

  • hi,

    如果是做光电检测不推荐使用光伏模式,建议使用跨阻放大器