各位老师好,用TLC2254设计仪用放大器时,在输入端输入一个几毫伏的信号,它的第一级放大输出信号怎么由几百毫伏慢慢的降为0了
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
仪表放大器虽然是放大差分信号,但是输入输入信号必须在其共模输入范围以内,例如您的电路是正5V供电,那么共模电压必须在0-5V以内,如果您直接将信号源接到两个输入端子是不能工作的,必须将信号源的地与你电路的地接到一起,或者使用浮地,就是在两个差分端子处分别对地接一个1M的电阻。另外,您为何要自己搭建仪表放大器呢,自己搭建仪表放大器要求R3和R7以及R4和R12严格匹配的,这样的电阻成本较高,电路也复杂,您可以使用INA333,INA118等集成仪表放大器来实现您的功能。