This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLC2254

Other Parts Discussed in Thread: TLC2254, INA333, INA118

各位老师好,用TLC2254设计仪用放大器时,在输入端输入一个几毫伏的信号,它的第一级放大输出信号怎么由几百毫伏慢慢的降为0了

  • 您好,能不能贴出电路呢,并附上详细说明?

  •  仿真是正确的,但是在板子上就不行了

  • yishun wang 说:

     仿真是正确的,但是在板子上就不行了

    hi,

    仪表放大器在使用的时候如果信号源没有接地注意在输入端提供额外的偏置电流回路。

  • 您好,它的输入是一个压力传感器,输出电压在20mv一下,有接地的。我测的时候把万用表挂在一级放大的两个输出脚,刚接触的时候有几百毫伏的电压,然后就一点一点的往下降,直到稳定在0点。每次测都是这种情况

  • 仪表放大器虽然是放大差分信号,但是输入输入信号必须在其共模输入范围以内,例如您的电路是正5V供电,那么共模电压必须在0-5V以内,如果您直接将信号源接到两个输入端子是不能工作的,必须将信号源的地与你电路的地接到一起,或者使用浮地,就是在两个差分端子处分别对地接一个1M的电阻。另外,您为何要自己搭建仪表放大器呢,自己搭建仪表放大器要求R3和R7以及R4和R12严格匹配的,这样的电阻成本较高,电路也复杂,您可以使用INA333,INA118等集成仪表放大器来实现您的功能。

  • 另外,仪表放大器的线性输入范围和共模电压以及差模信号大小及增益都是有关的,例如您的输入信号时20mV,另一端接地的话,共模电压才10mV,这样您电路中的前级的放大器输出会超出其电源范围的,所以是不能正常工作的,所以建议您给您的传感器提供适当的共模电压,最好是VCC/2,或者使用双电源供电。