Part Number: OPA171
OPA171最小检测差分电压是多少
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,这是一款输入电压能到负压轨的运放,同相端和反向端的输入电压范围为(V-)-0.1V~(V+)-2V .比如5V单电源供电,输入电压范围可以是-0.1V~3V的范围。

(V-)-0.1V,比如双电源+-10V供电,那么输入电压最低可以到-10-0.1=-10.1V,范围为(-10.1V~8V)。
同样比如+-5V供电,输入电压范围为(-5.1V~3V)。