This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA381: INA381 用于低端, 是否可以用于双向电流检测

Part Number: INA381


INA381  VCM 范围是-0.3V~26V,把它设计成低端检测,能否把它设计成双向检测(负压只用到-0.1V)

例如下面这样的设计,电流是双向的,sensor 0.5mΩ,电流170A