This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

如何搭建一个电流镜电路,用于复制SiPM的电流

硅光电倍增管(Silicon photomultiplier,简称SiPM)是一种高增益的光电转换器件。在我的电路中,共有16路SiPM并联,具有很大的结电容(4000pF×16片),输出电流范围大约为4mA~400mA。

如上图所示,这是一个SiPM的读出的ASIC电路结构。图中电流镜能够对SiPM的电流进行复制,并且可以按照一定比例缩小;我只需要进行精确的复制,请问Ti有合适的器件吗?