Part Number: LMH3401
在LMH3401EVM开发板上测试,单电源5V供电,VEE和GND接在一起。使用网络分析仪分析增益曲线,能够得到一个较好的曲线。
但是在自己的板子上,VCC接5V,VEE和GND直接接地,反向输入端直接50Ω接地,同相输入端直接接信号,CM端直接接一个2.5V。原本CM端是想通过AD端的输出进行动态调节,AD输出效果最优时,会提供一个1.7V的电压给到CM引脚,不知道是否能够这样应用?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LMH3401
在LMH3401EVM开发板上测试,单电源5V供电,VEE和GND接在一起。使用网络分析仪分析增益曲线,能够得到一个较好的曲线。
但是在自己的板子上,VCC接5V,VEE和GND直接接地,反向输入端直接50Ω接地,同相输入端直接接信号,CM端直接接一个2.5V。原本CM端是想通过AD端的输出进行动态调节,AD输出效果最优时,会提供一个1.7V的电压给到CM引脚,不知道是否能够这样应用?

自己板子上是这样的设置,断开右侧三个标记×的位置,SMA的一端接地,一端接到断开的这个位置,测得整体的增益曲线非常差,但是现在和开发板设置是一致的,请教是哪儿出现问题导致的?谢谢

您好,输出共模电压的范围(V+ – 2 V)~(V– + 2 V)。通常设置1/2的供电电压。所以5V供电,设置2.5V共模电压没问题。
电路没什么问题,我看到IN-端端接了50ohm阻抗,输入源也是50ohm阻抗吗?如果源阻抗也是50ohm,那就没问题。
除了增益曲线之外,输出波形质量呢?输出是否增益正确,曲线平滑?
很可能就是layout问题,我担心是layout时阻抗不匹配导致。
感谢回答:
1.请问如果我使用后端AD提供的1.7V的共模电压是否也是可以的?也是满足您所说的电压范围。
2.通过一个信号源,提供各个频率的正弦波信号,采集回来使用FFT分析,可以看到各频率信号的幅值,随着频率的提升,幅值会有明显的下降。频率范围是30-150MHz,按理说这个带宽内,增益曲线的平坦度应该是很好的,但是实际采集到的数据幅值却会有明显下降。
“For best harmonic distortion, maintain the CM input within ±1 V of the mid-supply voltage using a 5-V supply and within ±0.5 V when using a 3.3-V supply. The CM input voltage can be operated outside this range if lower output swing is used or distortion degradation is allowed. For more information, see Figure 18 and Figure 19. ”
按照手册中所述,我是5V单电压供电,中点电压是2.5V,那么我使用AD端动态调整输出的1.7V共模电压也是可以正常使用的吧?
Vcm的电压典型值为V- +1.6V~V+ -1.6V。然后再根据上述描述,为了更好的谐波失真,5V 供电,Vcm最好是维持在1/2VCC 的+-1V之内,即1.5V~3.5V范围内。所以根据这两个条件,1.7V 共模电压是可以正常使用的,没问题。

通过一个信号源,提供各个频率的正弦波信号,采集回来使用FFT分析,可以看到各频率信号的幅值,随着频率的提升,幅值会有明显的下降。频率范围是30-150MHz,按理说这个带宽内,增益曲线的平坦度应该是很好的,但是实际采集到的数据幅值却会有明显下降。
您指的是多大幅值? 要看下是不是收到压摆率的影响,大信号的幅值不仅仅和增益带宽积有关,还和压摆率SR有关。
SR=2*Pai*Vp*f
您好,运放输入端是一个±400mV的信号,信号可以调整频率,因为设计本身,需要在不同的频率下,信号整体幅值要保证在一条直线上。实际测试的时候,可以发现150MHz频率信号幅值差不多是30MHz信号幅值的56%,整体信号衰减明显。AD前端只有这么一个运放。
150Mhz或30Mhz频率没问题。
我想确认下,先别调整频率,单独测试,比如+-400mV输入,150Mhz的频率,能正常输出吗?或者30Mhz的频率呢?
我用TINA单独仿真这两个频率输出是都没问题的。
我是在原有TINA reference的基础上稍微改动了下,保证LMH3401的输入为+-400mV,150Mhz,Gain=2.仿真如下,基本上可以看到VM1差分输入+-400mV, Voutdiff=+-800mV输出: