This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH3401: 使用LMH3401 如何在单电源模式获得较好的增益曲线

Part Number: LMH3401

在LMH3401EVM开发板上测试,单电源5V供电,VEE和GND接在一起。使用网络分析仪分析增益曲线,能够得到一个较好的曲线。

但是在自己的板子上,VCC接5V,VEE和GND直接接地,反向输入端直接50Ω接地,同相输入端直接接信号,CM端直接接一个2.5V。原本CM端是想通过AD端的输出进行动态调节,AD输出效果最优时,会提供一个1.7V的电压给到CM引脚,不知道是否能够这样应用?