Part Number: XTR115

如上图,使用MCP4726数模转换芯片输出VREF(0-2.5V)控制电流环输出电流,现通过控制命令可以控制VREF输出0-2.5v的电压,但是XTR115的4脚IO输出端接的250欧姆负载两端的电压一直是3.5-3.8v跳变,请问以上硬件电路是否有问题?谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
使用MCP4726数模转换芯片输出VREF(0-2.5V)控制电流环输出电流,现通过控制命令可以控制VREF输出0-2.5v的电压
这里是指MCP4726的1脚VOUT控制电流环输出电流吧?VOUT输出电压0-2.5V?XTR115的3脚输入电流是多少?电流环您期望的输出电流范围是多少?
MCP4726的主控IC其供电电源是XTR115产生的吗?
请注意XTR115是2线变送器,其前端电路的电流消耗需要低于4mA,XTR115产生的电流环才能最低达到4mA,否则最小输出电流是前端电路的总供电电流。
通常,在XTR115的Vref和输入Iin管脚之间添加ROS电阻,以向XTR添加40uA偏移,这样当电压输入为0V时使其输出为4mA。如果没有ROS电阻器,当XTR的输入为0V时,电流输出将是XTR可以产生的最小输出。
单独给单片机电路用外接电源5V供电测得电流为17mA的。
这里的单片机5V电源是否与XTR115电路进行了隔离?如果单片机使用环路外电源供电,需要进行隔离 ,即XTR115 的3脚电流 IRET 不能引入环路外电流,具体见下面FAQ解释,第2个FAQ也给出了隔离电路连接示例。
[FAQ] The minimum output current of my 2-wire 4-20mA transmitter is greater than 4mA.
新的问题:两线供电12v,如果使用12v正端给内部稳压电源AMS1117-5.0供电,在经过LDO产生3.3v的电源个单片机电路供电,这样单片机电路可正常供电,但是XTR115的输出端接负载250欧姆时的电压一直是4V左右,如下电路,怎么改进?
如上所述XTR115是2线变送器,XTR115和前端电路的总电流需要低于4mA,否则的话电流环可以输出的最小电流是它们的总电流,即不能最小输出4mA。