This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA141: INA141可以用单端4.5V-36V供电吗,会不会对精度有影响

Part Number: INA141

  • 您好,

    从运算放大器结构上讲,运放在工作时无法分清自己是被双电源供电,还是单电源供电。任何运放的两个电源端,只要满足有足够的压差,运放就可以工作。不存在单电源专用
    运放,或者双电源专用运放。因此INA141使用单电源供电是可以的,但是信号输入和输出范围会受到限制。

    INA141不是轨至轨输入和输出运放,其输入和输出范围如下截图,因此单电源供电时其输入 0~2V以及(V+)-2V是不在输入范围内的;输出0~1.4V 和(V+)-1.4V是不在输出范围内的,这部分输入和输出不能线性工作。