This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教关于INA125仪表放大器测量电阻桥压力传感器的问题

  • 没有文字,我这里补充一下

    =============================

    我所遇到的问题是:在没有施加,或者施加较小压力的情形下,放大器输出大约80mV,直到施加压力大约2kg左右开始输出电压大于80mV,这样导致我不能够测量小于2kg以下的压力,我所使用的压力传感器最大量程30kg。我的应用要求能够测量到0.5kg或更小的压力,最大测量到25kg左右。

    不知道该如何来调整电路,能够满足我的应用要求?如果谁有好的建议或方案资料,可以发送到我的email:linearfly@163.com,谢谢!