Other Parts Discussed in Thread: OPA454
供电10V,200K电阻从电源到ED,其它都未接零件,我测试发现输入+,-端都有1.37V的电压,咋回事啊?这电压哪里来的?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: OPA454
供电10V,200K电阻从电源到ED,其它都未接零件,我测试发现输入+,-端都有1.37V的电压,咋回事啊?这电压哪里来的?
Hi Frank,
Thanks for your question.
For OPA454, the maximum E/D to E/D Com Voltage is 5V. It is NOT recommended to connect E/D to V+ through 200Kohms. Besides, it is NOT recommended to float amplifier input even if this amplifer is NOT used.
So please try to adjust your E/D voltage, and ground the input through pull-down resistor (if possible) to check if the circuit is ok? thanks.
Steven