Other Parts Discussed in Thread: ONET8501PB
RATE0和RATE1与SFF-8431的RS0 RS1是否有对应关系?按照SFF-8431的描述,应该在我RS0 RS1同为1的时候是最高速率选择,但ONET8501PB里面RATE0=0,RATE1=1的时候才有最高带宽9Ghz?这是否矛盾?我需要如何设置才能使之对应?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: ONET8501PB
RATE0和RATE1与SFF-8431的RS0 RS1是否有对应关系?按照SFF-8431的描述,应该在我RS0 RS1同为1的时候是最高速率选择,但ONET8501PB里面RATE0=0,RATE1=1的时候才有最高带宽9Ghz?这是否矛盾?我需要如何设置才能使之对应?
谢谢!
你好,ONET8501PB对应于MSA-8431协议中的Class I的功率需要标准,即全温度范围内小于1W的功耗。Rate selection这个功能是为了改善后级放大器的增益以提高系统噪声能力。这个功能对于FC应用是必须的。因为FC应用要求同时对2,4,8Gbps的带宽进行设定。Rate0/1和8431协议中RS0/RS1都是输入控制脚,并不是对应关系。你可以在I2C联通后,用软件进行带宽设置。
你好!
以SFF-8431中的SFP+为例,你说的RS0和RS1对应的是SFP+整个模块的一个输出引脚,其分别控制module receiver和transmitter的rate select, 而ONET8501只是ROSA部分的后级放大电路,RATE0和RATE1是用来控制ONET8501的带宽。ONET8501的RATE0和RATE1会连接到module中的微控制器,进行数据处理,而RS0和RS1是连接到微控制器的,故这两者之间没有直接的对应关系。
是可行的,留有rate0和1就是为了能够快速设置带宽。只不过通过寄存器可以设置更多不同的值,在实际应用中做微调,可以得到更好的性能。
再者,实际使用ONET8501PB时,I2C接口肯定已经连接。可以先通过rate0和1调,看实际情况定需不需要通过寄存器调啊。