马达类型为两相输入,行波型微型超声波马达。电机类型马达为压电超声电机,电机数量暂定为1个。芯片要求额定输入电压最好为12V以下,5V、3.3V、1.8V均可,对电流无特殊要求。芯片用来驱动单反镜头上的超声波马达,用TMS320DM368对驱动芯片进行控制。
芯片主要特性:1、能做到整步、半步和细分可调?
2、输出电流可调?
3、工作温度范围: -40℃ 至85℃
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.