This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于THS4303的输出失调电压问题

Other Parts Discussed in Thread: THS4303

在THS4303的datasheet上,我只是找到了输入失调电压,而没有输出失调电压,在实际电路的测试中,我发现电路的输出失调电压很大,想请问各位一下这种现象是否正常

测试电路示意图:

在输入端测得的波形:(在0电位附近没有偏移)

第一级运放输出波形:可以看到触发点的电位已经达到了14.5mV,说明一级的输出失调电压已经是14.5mV了

第二级运放输出:失调电压为82.3mV

请问这种失调电压的这种现象是否正常?

  • THS4303输入的失调电压典型值为1.5mV, 其固定增益为10,所以其输出的失调电压就达到了15mV,而从输入端测试结果看到,输入信号本身有100uV的直流电压,会和失调电压相互作用,所以输出为14.5mV是正常的,而第二级输出是有第一级的输出决定,因为第一级的输出作为第二级输入,和第二级的输入失调电压相互作用,经过放大后输出,所以输出82.3mV也是正常的。

  • 好的,谢谢,不过没想到级联后输出的失调有这么大……