This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于30MHz宽带放大器 THS3092

Other Parts Discussed in Thread: OPA2690, THS3092

各位专家您好!

现在我需要完成一个输入信号幅值为1V 频率为30MHz的正弦信号  通过放大器放大2倍

我按照官方数据手册的电路图连接如下:

大概在12MHz左右的输出信号就一定掉了一倍,请问THS3092的性能就应该是这样还是说我自己连接布线不好? 对于这种高频布线应该有什么讲究?另外用OPA2690可以完成这个功能嘛? 还有什么型号的芯片比较适合这个要求? 初学者请各位专家多多帮忙,谢谢!