Other Parts Discussed in Thread: OPA369, OPA727
已知输入范围为-5V至-4V,想选一种单端供电的运放来实现电压反向,不知道有没有这种芯片
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
您是要实现类似下面截图输入和输出吗?对信号频率有要求吗?


对于输入和输出信号范围,关键在于运放需要轨至轨输入和输出的,即输入信号需要包含0V,输出信号可以包含5V,下面OPA369运放虽然是轨至轨的,输入没问题,但输出不能完全到达电源轨,因此需要使用高于5V的电源供电。OPA369供电范围是VS = 1.7 V to 5.5 V,我使用的5.2V供电。如果5.2V电源不太好产生,也可以考虑使用大于5.5V供电范围的运放,比如 OPA727,这里我没有考虑信号频率,选择的时候,您还需要考虑信号频率。