This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PGA309: Register configuration problem

Part Number: PGA309

您好!我在使用PGA309配置寄存器时遇到了以下问题:

1、在没有外接EEPROM的情况下,是不是在Test Pin拉低时,vout一直都是高阻,得不到电压输出?

2、在Test Pin拉高的模式下,我可以通过单线或双线接口配置寄存器1和2的值,同时观察到vou有预期的电压值输出,但不能读取这两个寄存器的值,是不是这里只能修改可写寄存器的值而不能读取?

3、Test Pin拉高时,可以修改任何可修改的寄存器,我成功配置了寄存器12,但34寄存器却没有成功写入,vout没有变化。想问您,在没有外接EEPROM的情况下,可以修改寄存器34的值从而改变放大倍数得到预期输出电压吗?如果可以,出现这个问题的可能有哪些?

4、外接了EEPROM,但EEPROM里面没有预先配置值,是不是也不能使得PGA309test pin拉低时正常工作(vout有输出,寄存器可以配置)?

5、寄存器3不支持单线接口直接访问吗?以及pga309有内部存储器以供没有EEPROM外接时直接访问寄存器1234吗?

感谢您的解答!