您好,
請問OPA348工作在5.6V會有問題嗎? DATASHEET 上SUPPLY VOLTAGE是2.2~5.5 MAXIMUM RATING 是7.5V。 謝謝
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
通常情况下,我们建议参考推荐的电气参数范围,也就是说最好不要超过5.5V来保证参数的最佳性能,关于供电问题你也可以参考下面这个帖子,就是说超过5.5V但没有超过7.5V,甚至超过7.5V,还是可以正常工作的,但并不能保证芯片性能,并且长时间应用的话也有可能导致芯片损坏:
http://www.deyisupport.com/question_answer/analog/amplifiers/f/52/t/48090.aspx
即使是轨至轨输出,输出电压一般也是在电源轨的0.1~0.3V范围之内,所以5V供电的话,输出电压swing在-0.1~4.9V之间都是正常的。所以4.95V也是正常的。
楼主拿OPA348与AD8648相比,就类似于”拿小步枪与AK47相比一样“。
AD8648价格是OPA348的5倍。。。
楼主可以看一下OPA340的性能。谢谢!