Part Number: XTR111

1)以上电路,开始5引脚VREFG输出正常5.4V, 4引脚3V左右,6引脚从DAC给3.00V,输出12ma没有问题,板子电源和信号、加热供地,开启加热后,电流输出12ma正常,5引脚VREFG输出变成3.6V,电流输出12ma正常;片子稍微发烫;
2)以上电路,能不能直接用电流表测量输出电流 I1和AGND之间不串电阻,直接测试输出电流。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: XTR111

1)以上电路,开始5引脚VREFG输出正常5.4V, 4引脚3V左右,6引脚从DAC给3.00V,输出12ma没有问题,板子电源和信号、加热供地,开启加热后,电流输出12ma正常,5引脚VREFG输出变成3.6V,电流输出12ma正常;片子稍微发烫;
2)以上电路,能不能直接用电流表测量输出电流 I1和AGND之间不串电阻,直接测试输出电流。
您好,
1、
板子电源和信号、加热供地,开启加热后,电流输出12ma正常,5引脚VREFG输出变成3.6V,电流输出12ma正常;片子稍微发烫;
您这里是将电路板放在高温老化房验证电路板的高温工作情况吗?测量5引脚VREFG输出变成3.6V时,4脚电压是多少?
2、XTR111是恒流输出,正常情况下是可以短接负载的。实际短接的时候需要考虑R77和Q8等回路中的元件是否可以承受得了流过电流时产生的功率,避免烧毁元件。