Part Number: AMC1200
如下图,
当输入是0.16v,输出是1.91v,放大倍数是11.93倍
当输入是0.08v,输出是1.6v,放大倍数是20倍
当输入是0.032v,输出是1.4v,放大倍数是43.75倍
请问这是什么原因?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,几种输入都是符合输入共模电压以及差分输入电压要求的,建议将输入端滤波器的R18和R21的阻值换到24ohm以下,datasheet中使用的12ohm。
更换这里的电阻,再验证是否符合增益要求。
这款隔离放大是单电源供电的。high side和low side各自有自己参考的GND pin。
输入的共模电压范围只要在-0.16V~VDD1范围内即可,VID差分输入为典型值 +-250mV,最大为+-320mV,所以您给的三次输入都是满足这个输入要求的,能保证其工作在线性区域。 有换一片试试吗?

输出侧供电电压改为5v
您好,输出端改5V,怎么样了?VCC2的电压范围2.7V~5.5V,所以3.3V也是没问题的,因为您的这几种输入还不会导致输出饱和状态,即使饱和,输出也是削波现象,放大倍数不会改变。