This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

低频带通滤波运放选择

Other Parts Discussed in Thread: LMP7731, OPA4348

现需要一款运放,构成中心频率为1Hz,带宽为5hz,放大倍数为10的带通滤波器,输入信号为几mv的交流电压,要求运放性能优异,噪声小,采用单电源3.3V供电。请教能不能给提供几款TI的运放供选择。谢谢!

  • 你好,

    LMP7731噪声性能不错,但不知道你的具体要求是多少精度,对失调等其他参数有啥系统级要求么。是ECG里用么?方便说下应用场景么,可以让同事更好推荐合适产品。

    另外感兴趣一点是,中心频率1HZ怎么做出5HZ带宽的滤波器...比较疑惑。不过这个不那么要紧,因为现在一般的运放在带宽和压摆率都能满足。

  • 谢谢你的建议。这个主要是想应用在对红外探测器的输出信号进行滤波、放大,探测器出来的信号是一个带有直流电压偏置幅值为几mv,频率为1Hz的交流电压信号。因为电路板尺寸的制约,我自己看了一个运放OPA4348四运放。请教下这个单电源运放使用时,应该注意哪些地方?其实我是想先通过带通滤波得到以1Hz为主的交流信号,然后对其进行放大,能不能给些实际应用的建议?谢谢!

  • 可以使用TI的filter pro免费软来进行设计滤波器。然后单电源使用应该注意加直流偏置。看看其他人有补充么。