Other Parts Discussed in Thread: OPA656
信号通过BNC进入PCB,输入阻抗为1M欧,采用OPA656构成电压跟随器,测试信号通过BNC后的情况,原理图和仿真结果如图
设计输入信号带宽大约100M,可糟糕是我用示波器实测该点信号,1M开始往后衰减的就特别厉害,请问遇到这个问题该怎么办?非常感谢~
实测的时候信号源为高阻输出,PCB为4层板,如果需要,可以附上BNC处的PCB设计。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: OPA656
信号通过BNC进入PCB,输入阻抗为1M欧,采用OPA656构成电压跟随器,测试信号通过BNC后的情况,原理图和仿真结果如图
设计输入信号带宽大约100M,可糟糕是我用示波器实测该点信号,1M开始往后衰减的就特别厉害,请问遇到这个问题该怎么办?非常感谢~
实测的时候信号源为高阻输出,PCB为4层板,如果需要,可以附上BNC处的PCB设计。
datasheet上不是说能达到500M么,1M欧电阻是BNC输入阻抗,不能更改。
我怀疑是不是驱动电流不够,后级负载输入阻抗是200欧,最大输出电流是70mA,不知道能不能帮我测试一下,我这边工具太少,不方便调试,非常感谢~
如果真的是驱动电流问题,能不能推荐一款适合做电压跟随器的运放,带宽100M以上,驱动电流大的
200欧和70mA电流是14V的电压,超过电源轨。你能确定是这个值吗,如果是要到14V那就必须换了。
一般用SR来算大信号的带宽,大信号带宽由SR决定,小信号带宽由GBW决定。SR>2*PI*f*A; A是输出幅度,f是最高频率,PI是圆周率。
还有个好方法测试下是否是1M欧姆电阻的问题,就是直接换个100欧姆电阻试试带宽有宽么?