This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TI型号中E4,G4到底有什么含义?

TI专家好,

TI型号中E4,G4到底有什么含义?比如TL062CDE4,TL062CDG4有什么区别呢?

谢谢!

  • 请参考这里:

    http://focus.ti.com/quality/docs/gencontent.tsp?templateId=5909&navigationId=11753&contentId=5055

  • 注意看这里:

    :Beginning June 1, 2004, TI will change the "e" in the Pb-free finish category to a "G" when a TI device/package combination converts to a "Green" mold compound. For example, a TI device built with NiPdAu finish will have a Pb-free finish category of "e4" until a green mold compound is implemented. When implemented, the Pb-Free finish category will be changed to "G4". (Replacement of the "e" with a "G" in the Pb-Free finish category is not part of the J-STD-609 standard at this time, but will be implemented for TI products.) "G3" category is "E3" matte tin (Sn) Pb-free finish with "Green" mold compound

    即2014年6月1号之后G4就是之前的E4,名字变了,芯片本身并没有什么变化

  • E4和G4分别代表的是绿色环保和无铅产品,事实上,目前二者已经没什么区别,因为大多数产品都是绿色无铅的,除非有特殊说明的。

  • e4:管脚镀层 NiPdAu,NiPd,Au,Ag(Pb-Free+250C/260C MSL)

    G4:管脚镀层 NiPdAu,NiPd, Au,Ag (sameas e4 + Green Mold Compound)