Other Parts Discussed in Thread: ISO124
我在使用ISO124做一个数据采集系统,由于ISO本身的失调电压为20mV左右,对采样精度的影响比较大,请问有没有什么方法可以减小失调电压的影响?谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: ISO124
我在使用ISO124做一个数据采集系统,由于ISO本身的失调电压为20mV左右,对采样精度的影响比较大,请问有没有什么方法可以减小失调电压的影响?谢谢
是否可以先采样后隔离?这样选用低失调和低漂移的芯片并上ADC在同侧,然后用ISO74xx系列的数字隔离器进行隔离传输到MCU端,这样采样精度可能会有所改善。
交流信号的频率范围是多少?如果交流信号的最低频率距离DC较远,可以考虑用一个电容挡掉直流成分。
TI最新的隔离运放AMC1200的失调电压最大值1.5mV,不知道是否满足要求,如果要求较高,推荐推荐先采样后数字隔离的方案
你好,
根据所需要处理的信号频率,用100uF左右电容(50Hz时阻抗约30ohm)隔直后,加一个几k欧姆的对地电阻,再挑选一个offset小的运放做缓冲器,以保证最终不影响AD的采样精度。
使用大电容的交流耦合可能带来较大的相位误差,在采集系统中需要考虑到这个因素。