本人现在用TI公司的SA5532放大一个50HZ的工频信号,输��范围为40mv到5V,输出最大为14V峰峰值,用20V给sa5532供电,输出失真,峰值顶端到峰值左边谷值在X轴上的△X=9ms,峰值顶端到峰值右边谷值在X轴上的△X=11ms,波形峰值向左边偏移,是什么原因造成的呢,困扰很久了。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
本人现在用TI公司的SA5532放大一个50HZ的工频信号,输��范围为40mv到5V,输出最大为14V峰峰值,用20V给sa5532供电,输出失真,峰值顶端到峰值左边谷值在X轴上的△X=9ms,峰值顶端到峰值右边谷值在X轴上的△X=11ms,波形峰值向左边偏移,是什么原因造成的呢,困扰很久了。
信号的直流放在多少?直流是0V吗?负载端挂了什么样的负载?这个芯片的输出级是个class AB,看上去你的电路是出现了一些非线性的成分,可能和输出级的直流电平有关。
信输入信号的直流偏置为芯片供电电压的一半,负载是一个100K的电阻
信输入信号的直流偏置为芯片供电电压的一半,负载是一个100K的电阻
信输入信号的直流偏置为芯片供电电压的一半,负载是一个100K的电阻
可以考虑一下,把输出端的直流电压向上抬一点,或者向下压一点,看看是否可以改善。另外,可以把电路图或者TINA模型发上来吗?
好像上传不了附件,我试一下,如果不行你能不能留个邮箱呢,我发邮件给您,谢谢
上升沿下降沿不一样,二边不相等,电路图里面是没有100K的负载的,后来在电路板上加的

测一下运放1的输出和运放2的输出,看看失真是发生在哪一级
信源到第一级输入只经过了一个高通滤波,看上去不应该有失真,你的电容和电阻取值多少?9V的直流旁·有没有加滤波电容?信源是否干净?
输入信号的交流耦合的电容是4.7UF的,9V的上拉电阻是10K。9V的输入电压纹波很小,20mv以内,信号源也很干净,会不会是第二级放大对它造成影响呢,明天再去试一下把第二级断掉看看会不会失真,谢谢!
4.7uF电容,10K电阻在50Hz处有大约10dB衰减,你的高通滤波器可以有更低的截止频率。
那么应该怎么解决呢,衰减应该是把信号的幅值降低,会影响到波形失真吗?我也试过把10K的电阻改为100K,输入电容容值增大,好像也没什么效果
把10K电阻改成100K,在50Hz附近衰减大约0.2dB。