OPA241一般应用在什么场合呢?
电路中的传感器输出信号为0-300nA,尝试过很多次,使用OPA241无法放大该信号,输出端无输出,请问有人遇到类似情况吗?
一些说明(请见下图):
1)传感器输出为0-300nA电流信号;
2)场效应管防止漂移;
3)T1为1.2V稳压管;
4)电位器R10用于调零;
5)电阻R12与电位器R11用于放大信号。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
首先OPA241是单电源通用放大器,当然能够放大小信号,但是您这个电路时电流/电压转换电路,输入电流较小,需要注意的是,首先为了保证良好的精度需要选择场效应管型的放大器,241是双极型放大器,输入偏置电流较大,您可以选择OPA171,OPA320等等。
其次您要注意您传感器输出电流时正电流还是负电流,因为电流/电压转换电路是反相的,如果输出正电流的话放大器就需要双电源供电了。
您好,传感器1脚输出电流,并且传感器输出的是直流电流,则不用反相,看你的电路接的是对的,不用再反过来。
首先,非常感谢您的建议!
根据您的分析,确实是因为运算放大器的问题,更换为场效应管型,就很灵敏。
在这种微小信号放大的场合使用OPA241,不仅贵,而且效果不好,走了弯路。