Other Parts Discussed in Thread: OPA564, OPA1652
信号输入侧条件:
a) 输入信号幅值为3V左右;
b) 输入信号频率为3KHz~500KHz;
c) 信号源阻抗为2KΩ;
运放输出侧要求:
a) 输出信号幅值达到VCC(8~20V);
b) 负载阻抗为1~100Ω;
c) 输出功率达到5W。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你可以考虑OPA1652,轨至轨输出,比较宽的供电电压范围±2.25 V~ ±18 V, 或者+4.5 V~ +36 V。
您好,
1,直流电源给的功率取决于您信号的大小和负载大小,例如您输出3V,负载6欧,电流就为0.5A,因此直流功率为6W。
2,这个完全取决于您的负载,例如对于1欧,那么受最大电流(1.5A)限制,最大输出峰峰值为3V,因此可以计算功率,但对于大电阻负载来说,主要受摆幅限制,12V供电,OPA564在输出正负轨会有1-2V的摆幅限制。
3,564就是典型的AB类功放输出,您可以参考相关资料。
4,增益是由您自己设置的,和运放一样使用,其增益带宽积为17MHz,过大的增益会降低有效带宽。
5,如4所示。
您好,
您可以采用这个电路,我现在无法给你非常精准的参数,但是有一些指导法则,因为很多电路需要反复调试才能达到预期效果的。
1,首先12V供电,是没有办法输出12信号的,虽然564摆幅非常优秀,但是还是会有一些摆幅限制的,您可以参考datasheet中OUTPUT这一项参数,摆幅是和输出电流有关的。
2,关于R1和Rf的选择,增益为-Rf/R1,所以选定一个就可以了,那么怎么选呢,由于您信号的带宽很宽,频率也比较高,所以这两个电阻尽量选小一些,不然会影响带宽,例如R1取1K,或者更小一点的。
3,C1的选择完全取决于R1,因为C1和R1构成高通滤波器,R1取1k时,C1可以取104。
4,Cf是相位补偿电容,但同时也会和Rf构成低通,因此他们的频点应在5MHz左右,例如Rf为3k,Cf可以取10pF左右。
TI专家好!
在实验室试验时,将OPA564芯片的电路设计这样,基本满足功能测试需要,但应用到产品中,总感觉应该还需再做些优化改进,才能将芯片功能发挥到极致,望专家给指点下。
您好,首先您的电路时反相电路,你的输入偏置是正的还是负的呢?第二您带的负载多大, 因为您的理论输出信号是10.8V峰峰值,您要参考datasheet,考虑摆幅的限制。