技术专家,您好!
现本人想制做一种信号放大器,要求:
1、独立的电压放大通道,输入为模拟小信号,输出电压:0~100V,频带为0~1MHz,要求 输出信号可带20mVA的小负载;
2、独立的电流放大通道,输入为小信号输入,输出电流0~5A/1A,频带为0~1MHz, 输出信号可带1VA(5A情况下)或0.4VA(1A情况下)的小负载。
各位专家能否提供技术支持和解决方案? 盼回复,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,
1、独立的电压放大通道,输入为模拟小信号,输出电压:0~100V,频带为0~1MHz,要求 输出信号可带20mVA的小负载;
A:实现高的电压输出和带宽,你可以通过运放输出来控制后端MOSFET推挽电路来实现,但需要考虑slew rate 和GBW。
2、独立的电流放大通道,输入为小信号输入,输出电流0~5A/1A,频带为0~1MHz, 输出信号可带1VA(5A情况下)或0.4VA(1A情况下)的小负载。
A:可考虑把小信号输入到运放,通过运放输出端去驱动后端晶体管基极(栅极),实现扩流的目的。