This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

纽扣电池经过不工作运放,电量不久就消耗完的疑问



想请问TI的专家,我现在用纽扣电池给ARM供电,它在没有控制电的时候起作用,给RTC时钟供电。现在发现一个问题,就是电池很快就消耗完,目前感觉原因出现在如图所示问题中。VBAT是给ARM供电,AD_BAT是采集电池电压,现在的问题是当我不串2M电阻,直接将3V电压引到运放时,电池没过多久就消耗完。看了一下所用运放的参数,输入阻抗也很大,不应该消耗很大电流。电池工作时,运放是不工作的,没有3.3V控制电。难道是运放不工作时,他的输入引脚会有很大的灌电流,还是运放不工作时,输入阻抗会变化?请TI的专家帮忙解答下,谢谢!