业务需要产生一个上升时间为400ns,下降时间为80ns,低电平为0V,高电平为1V的锯齿波,具体情况如下所示。求助。。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我之前做过一个该锯齿波的产生电路具体方案如下:
1、用555定时器产生一个占空比可以变化的方波(或者产生的方波进入高速比较器,变成比较好的方波)
2、用运放产生一个加法/减法电路,移位方波的低电平。使得最终的高低电平产生一定的比例(比如这块上升要求400ns,下降80ns,我就使得上升时间/下降时间=5)
3、将2产生的矩形波信号接入积分电路中,即可完成该电路的操作(因为要求是低电平为0V,该积分电路就必须有箝位电路)。
箝位我采用了二极管箝位限压电路,效果不好,可能是由于二极管的结电容比较大,导致波形有负向到0慢慢过渡的一条曲线。一直没有找到特别好的箝位电路,所以一直放着了,您有什么好的建议吗?